top of page

Mobile Robot Platform Guide for Physical AI Research

  • Sep 1
  • 12 min read

A mobile robot can expand physical AI research beyond a fixed workstation, but mobility alone does not make a platform suitable for your experiments. The right choice depends on where the system will operate, what it must manipulate, how observations will be captured, and how those datasets will support training and evaluation.

The best mobile robot platform is the one whose mobility, manipulation, sensing, compute, and data systems match a defined research workflow. Start with the environment and task, then test whether the platform can support repeatable experiments from teleoperation and data capture through model development.

That means treating the robot as research infrastructure rather than a collection of specifications. A platform intended for controlled lab work may need different capabilities from one used across field environments, especially when consistent arm and camera placement matters between sessions. The decision becomes clearer when you define those operating conditions and success criteria first.

What Should You Define Before Choosing a Mobile Robot Platform?

The strongest platform decisions begin before anyone compares motors, sensors, or software stacks. Define the environment and task first, then translate those requirements into mobility, manipulation, sensing, compute, data capture, software compatibility, and a deployment path. This sequence keeps the platform aligned with the experiment instead of letting a product specification define the research question.

Start with the task, environment, payload, operating mode, and evaluation boundary. Then select the platform capabilities that support the work you need to repeat, measure, and extend.

Define the task and environment

Write down what the robot must do and where it must do it. A controlled lab with a known floor, fixed workstations, and repeatable lighting creates different requirements from field work across changing rooms or locations. Specify surfaces, thresholds, slopes, workspace dimensions, obstacles, lighting, network access, and whether people will share the operating area. A mobile robot can move through its environment, but mobility alone does not provide navigation, autonomy, or a solution to sim-to-real challenges. Those boundaries should remain explicit in the requirements.

Also decide whether the project needs a mobile base at all. Mobile field work and controlled lab work are distinct research contexts. Trossen positions Mobile AI for field work where arm and camera placement should remain consistent between sessions, while Stationary AI is intended for a controlled lab environment. The right choice depends on whether moving the system is part of the research problem or simply adds integration work.

Quantify payload, power, and movement

List everything the platform will carry, including batteries, computers, sensors, fixtures, tools, and any manipulator. Plan for the complete operating load rather than the payload of the base alone. A useful early design question is whether the system must carry a light sensor package or a substantially heavier research configuration. Payload planning and power planning are linked: estimate the voltage, current, battery capacity, duty cycle, and recharge process required for a full session. These requirements should be documented before selecting a base; design guidance commonly treats both carried load and power as first-order decisions (mobile robot platform design guidance).

Specify how movement will be controlled. A differential-drive base with tank steering may suit a controlled experiment, while another project may require a different drive architecture. Do not treat a mobility mechanism as proof of autonomy. Define whether operation will be manual or teleoperated, cloud-operated, autonomous, or a staged combination of these modes. Finally, define success before procurement: which task episodes, surfaces, distances, payloads, data outputs, and repeatability measures will determine whether the platform is useful? Include early durability testing in that plan, since a chosen platform should be validated under the conditions it is expected to support.

Mobility: Wheels, Tracks, Legs, and Navigation

Answer: Choose locomotion by matching surface conditions, payload, endurance, and control requirements to the experiment. Wheels are usually efficient on predictable floors, tracks favor traction and stability on uneven ground, and legs expand terrain access at the cost of mechanical and control complexity. Navigation is a separate systems problem from simply moving the base.

A mobile robot is defined by its ability to locomote rather than remain fixed in one location. In practice, that means evaluating the base as part of a complete system that includes actuators, sensors, a controller, and a power system, not as an interchangeable chassis. The right choice depends on where the robot will operate and what it must carry or position repeatedly. Mobile robot architecture and locomotion overview.

The table is a starting point, not a substitute for testing. Measure the surfaces, clearances, payload, and turning space that define your experiment.

Environment determines the useful mobility

For a controlled lab, a wheeled base may provide the repeatability needed for positioning sensors or manipulation hardware. Field work can introduce thresholds, irregular surfaces, changing layouts, and obstacles that alter the balance between wheels, tracks, and legs. Treat those conditions as test requirements, rather than assuming that a more complex mobility mechanism is automatically better.

Payload and power belong in the same calculation. Plan for the full carried load, including arms, cameras, compute, batteries, and accessories. Mobile systems commonly use DC battery power, so the battery must support the intended duty cycle while leaving capacity for manipulation and sensing. Power requirements should be established early, and the selected platform should undergo durability testing before a research workflow depends on it. Mobile platform design considerations.

Navigation is not the same as autonomy

A platform may be manually teleoperated, follow a predefined route, use guarded obstacle avoidance, or operate with a more autonomous navigation stack. These modes imply different sensing, localization, safety, and validation requirements. A mobile base alone does not solve navigation, autonomy, or sim-to-real challenges. Define whether the experiment needs repeatable teleoperation, supervised movement, or autonomous behavior, then select the sensors and software needed to test that mode honestly.

How Much Manipulation Capability Does the Platform Need?

Answer: Match the arm to the physical demands of the experiment, including the number of independent motions. Object weight, workspace, sensing and feedback needs, and whether the task requires one or two arms. A mobile base adds value only when the manipulation system remains capable and repeatable as the platform moves between work areas.

Start with the task rather than the arm catalog. A platform intended to open containers, reposition objects, or collect demonstrations may need a different workspace and end-effector strategy than one designed for simple pick-and-place. Define the objects, grasp types, contact forces, approach angles, and maximum load. Then check whether the arm can reach those poses without operating at the edge of its workspace.

Degrees of freedom, or DOF, determine how freely the end effector can orient and position itself. The WidowX AI arms used in Trossen's mobile AI research platform provide six degrees of freedom. That articulation supports varied approach angles and orientation changes, but DOF alone does not guarantee task success. Payload, reach, mechanical stiffness, gripper design, and the quality of the control loop all matter.

Check payload, reach, and shared workspace together

Payload should be evaluated at the point where the arm will actually work. The WidowX AI specification lists a 1.5 kg payload at full extension and a 700 mm reach. Those values provide useful boundaries for experiment design, but they should not be treated as a universal working envelope. Objects, grippers, acceleration, and the distance from the base can change the practical margin.

For bimanual research, measure the combined workspace rather than assessing each arm independently. The WidowX AI configuration has a fully extended span of 1400 mm. That span helps teams reason about hand-to-hand coordination, object presentation, and camera placement. It also makes fixture dimensions and collision checks part of the platform decision. If the arms cannot reach the same object comfortably, a nominally bimanual setup may create inconsistent demonstrations.

Keep this article's platform-level decision separate from arm-only selection. If the main question is which manipulator best fits payload, reach, end effectors, or contact experiments, use the dedicated mobile manipulation robot selection guide rather than duplicating that narrower framework here.

Feedback and repeatability shape usable data

Manipulation research depends on more than an arm reaching a pose once. Repeated episodes need responsive control and observable state. QDD actuators, hardware-based gravity compensation, 500 Hz position feedback, and torque feedback up to 16 kHz are documented features of the WidowX AI arms. These capabilities can support experiments that examine contact, force response, and repeatable teleoperation, provided the rest of the system and task design are controlled.

Field work adds another requirement: arm and camera placement should remain consistent between sessions. That is a stated use case for Mobile AI. For a deeper manipulation-specific buying framework, see the mobile manipulation robot guide. Here, keep the decision broader: select manipulation capability as one part of the platform's mobility, sensing, compute, and data workflow.

Sensing and Onboard Compute for Physical AI Research

Answer: Choose sensing and compute around the observations, control loop, and evaluation process your experiment requires. RGB-D coverage, stable camera placement, an operator interface, and a deliberate split between local and cloud resources matter more than a mobile base alone.

Start with the viewpoint, not the camera count

A useful sensing configuration should make the task observable from the viewpoints that matter. For bimanual manipulation, that may mean seeing both end effectors, the workspace, and the object being handled without allowing one arm or the operator to obscure another. Camera placement also affects repeatability. Mobile AI is intended for field work where arm and camera placement remain consistent between sessions. Consistent placement helps researchers compare demonstrations and evaluate changes without rebuilding the observation setup each time.

Mobile AI includes three Intel RealSense D405 cameras with RGB-D depth sensing. The cameras provide an 87 by 58 degree field of view and capture at up to 90 FPS. Those specifications give a research team useful options for arranging multiple viewpoints and collecting depth information alongside color data. They do not, by themselves, determine whether a setup is adequate. Validate occlusion, working distance, lighting, depth quality, and the portion of the workspace visible during the actual task.

Match frame rate and control to the experiment

Frame rate should serve the motion and measurement problem. A high capture rate can help describe faster interactions, but it does not replace synchronized streams, consistent camera geometry, or a clear definition of the episode being evaluated. Similarly, a touchscreen can improve local control and make an integrated platform easier to operate in the field. But the interface should support the research workflow rather than become the workflow. Mobile AI pairs its three cameras with a 10-inch touchscreen and two Leader-Follower WidowX AI arm pairs, giving researchers a compact configuration for teleoperation and data collection.

Separate local iteration from larger training runs

Onboard compute is valuable when researchers need to collect data, teleoperate, and test a model near the robot. With the laptop configuration, Mobile AI supports on-device ACT and ACT++ model training, cloud model training, and model evaluation for ACT and ACT++ models. This creates a practical division of labor: use local resources for rapid checks and shorter iteration loops, then use cloud resources when experiments require more capacity. Keep that boundary explicit in your protocol so a result is tied to the model, data, and evaluation environment that produced it.

A mobile robot platform can carry sensing and compute into a new workspace, but mobility does not guarantee navigation, autonomy, or a successful sim-to-real transfer. Those remain separate research questions. Define them, test them, and document their limits alongside the sensing and compute configuration. The Trossen Robotics documentation can help teams inspect the available hardware and software interfaces before committing to an experiment.

Data Capture and Software Compatibility

Answer: A useful mobile robot platform should preserve synchronized sensor and robot-state data, organize each episode with searchable metadata, and move cleanly from teleoperation to training and evaluation. Software compatibility matters because a capable base is only as valuable as the dataset and models your team can reproduce with it.

Start by treating every demonstration as a structured experiment rather than a video recording. Multi-camera synchronization keeps observations aligned with robot actions, while episode metadata and indexing make it possible to find, filter, and compare demonstrations later. The Trossen data collection SDK supports these functions, records sessions in TrossenMCAP, and exports data to LeRobot V2 format. That gives a research team a durable capture format and a path into model-development workflows without rebuilding its data pipeline for every study.

This architecture is especially important when a platform moves between environments. Consistent data structure helps teams compare demonstrations collected in different locations and inspect failed episodes. It also helps identify whether a result reflects the task, the operator, the camera view, or the robot state. The same structure supports a more disciplined robot teleoperation for data capture process, in which repeatable demonstrations become training assets rather than isolated trials.

Check the full software path, not just the interface

Compatibility should be evaluated across the entire stack: hardware, real-time drivers, data pipelines, ROS 2, LeRobot or OpenPi, and the user application or machine-learning model. Trossen documents this layered architecture and provides guides through its Trossen Robotics documentation. ROS 2 can connect robot control and application components, while LeRobot and OpenPi provide relevant framework paths for learning-oriented workflows. The practical question is whether your existing code, data schemas, and evaluation tools can connect at each layer with limited custom integration.

Simulation can extend that path before hardware testing. Documented environments include MuJoCo, NVIDIA Isaac Sim, Gazebo, and distributed Grid training environments. Simulation does not eliminate sim-to-real work, and a mobile base alone does not solve navigation or autonomy challenges. It can, however, give teams a controlled place to test software interfaces, task logic, and data-handling assumptions before collecting more physical demonstrations.

The resulting workflow is coherent: teleoperate the robot, capture synchronized multimodal observations. Annotate and index episodes, export a compatible dataset, train a model, and evaluate it against repeatable tasks. That is the difference between selecting hardware that merely moves and selecting a research system that supports a complete physical AI workflow. Open research platforms illustrate the range of this ecosystem, from Robotont 3, a 3D-printable ROS-supported platform, to Robot DE NIRO, a human-centered autonomous mobile research platform. The right choice depends on your experiment, but the data path should be explicit before procurement.

Deployment Readiness: Support, Testing, and Scale

Answer: A deployment-ready mobile robot platform is not defined by mobility alone. It should withstand representative use, remain serviceable, support a repeatable operating workflow, and make its limits clear before a research team treats a demonstration as autonomy.

Use the following checklist before expanding from a promising experiment to a sustained research program. Trossen's SLATE is a useful example of a low-profile UGV for teams that need substantial carried capacity alongside a mobile research workflow. The documented platform provides zero turning radius, a 70 kg payload capacity, 10 to 12 hours of battery runtime. Compatibility with the Trossen Data Collection SDK, replacement parts for user repair, and a one-year warranty. Treat those published characteristics as starting points for validation against your own payload, terrain, duty cycle, and sensing plan.

  1. Test durability under the real workload.

    Early testing should assess the durability of the platform you have selected or built. Do not limit validation to a successful first run. Exercise the base, mounted hardware, cable paths, sensors, and manipulation components through representative cycles. Include the surfaces, payloads, operating duration, and repositioning that your study actually requires. Record failures and maintenance needs, then repeat the test after corrections. This creates evidence about reliability without confusing a short demonstration with production readiness. The underlying testing principle is documented in the

    mobile robot platform design guidance

    .

  2. Check serviceability and technical support.

    Identify which components can be inspected, replaced, recalibrated, or updated without redesigning the system. Documentation should cover hardware, software, and development interfaces, as illustrated by the

    AgileX LIMO documentation

    . Also confirm how technical questions are handled over a longer project timeline. Trossen states that its Promise includes lifetime technical support from U.S.-based engineers, a 48-hour response commitment, and escalation access for complex issues. That kind of support matters when a lab must preserve a dataset schedule or keep multiple researchers productive.

  3. Make the workflow repeatable.

    Define the sequence from setup and teleoperation through synchronized data capture, training, evaluation, and deployment. Fix the physical configuration where consistency matters, document startup and recovery procedures, and record the conditions for every episode. A practical

    robot learning lab setup

    should make it easy for another operator to reproduce the experiment rather than depend on undocumented expertise.

  4. Choose the operating mode explicitly.

    Decide whether the platform will be manually teleoperated, cloud-operated, autonomous, or used in more than one mode. Each mode changes the requirements for communications, supervision, safety, testing, and failure recovery. Treat autonomy as a capability to validate, not a label inherited from the presence of a mobile base. A mobile base alone does not solve navigation, autonomy, or sim-to-real challenges. Define the environments and tasks where the system is expected to work, then state the conditions where human control or intervention remains necessary.

  5. Plan the scale-up path.

    Before purchasing additional units or moving into field work, compare the tested workflow with the demands of more operators, longer sessions, new environments, and larger datasets. Confirm that support, documentation, service procedures, and software interfaces can sustain that expansion. A platform is ready to scale when the team can explain what is repeatable, what still requires supervision, and what evidence is needed before claiming broader deployment.

Frequently Asked Questions

What should you include in a mobile robot platform budget?

Budget for more than the base. Account for manipulation hardware, cameras and other sensors, onboard compute, batteries, mounting or safety equipment, software integration, data storage, operator tools, maintenance, and support. The right comparison is the cost and effort required to produce repeatable research data, not the purchase price alone.

Should a research platform be designed for indoor or outdoor use?

Start with the environment where the experiment will run. Indoor lab work may prioritize precise maneuvering, repeatable camera views, and integration with controlled workspaces. Outdoor or field work adds uneven surfaces, changing lighting, weather exposure, longer operating distances, and recovery requirements. A mobile base does not automatically provide navigation or autonomy, so define those requirements separately.

Are wheels or tracks better for a mobile research robot?

Wheels are often a practical choice for smooth floors, efficient movement, and straightforward indoor testing. Tracks can provide more contact with the ground and may suit loose or uneven terrain, but they can add mechanical complexity and affect turning behavior. Choose the drive system from measured terrain, payload, clearance, maneuvering space, and battery requirements rather than treating one option as universally best.

When does a mobile platform need manipulation capability?

Add an arm when the research task requires the robot to reach, grasp, reposition, or interact with objects after it moves. If the experiment only concerns navigation, inspection, or sensing, a mobile base with the required sensors may be sufficient. For physical AI research, also evaluate arm workspace, payload, feedback, teleoperation, and whether the platform keeps sensor and arm placement consistent across data-collection sessions.

Choose a Mobile Robot Platform With a Clear Research Path

A well-matched platform can help your team move from hardware evaluation to repeatable physical AI experiments with fewer integration questions. Trossen Robotics can help you connect mobility, manipulation, sensing, compute, and data capture requirements to a practical research setup.

Contact Trossen Robotics to discuss your mobile robot platform requirements and get a research-ready recommendation or quote.

 
 
 

Comments

Rated 0 out of 5 stars.
No ratings yet

Add a rating

OUR PROMISE TO YOU

We stand behind our products with an industry-leading commitment to reliability, service,
and long-term support—because we believe performance should be measured in years, not months.

BUILT FOR REAL-WORLD RESEARCH ENVIRONMENTS. COVERS DEFECTS IN MATERIALS AND WORKMANSHIP. WEAR COMPONENTS ARE FIELD-REPLACEABLE AND READILY AVAILABLE.
LIFETIME SUPPORT FOR TROSSEN PRODUCTS 

Follow Us On Social

  • LinkedIn
  • Youtube
  • Facebook
  • GitHub
  • Twitter
  • Instagram
  • TikTok

© 2026 Trossen Robotics. All Rights Reserved.

bottom of page