Aloha Is Now Trossen AI: The Evolution of Affordable AI Research Hardware
top of page

Aloha Is Now Trossen AI: The Evolution of Affordable AI Research Hardware

  • Writer: Marc Dostie
    Marc Dostie
  • Mar 4
  • 4 min read
Aloha is now Trossen AI

Since its inception, Aloha has been synonymous with affordable, high-performance hardware for robotic machine learning research. Built around the mission of A LOw-cost HArdware, Aloha enabled countless students, researchers, and engineers to push the boundaries of AI and machine learning. But as the field of robotics and artificial intelligence continues to evolve at an unprecedented pace, so must we.


We’re excited to introduce Trossen AI, the next evolution of our research hardware. Trossen AI builds upon the foundation of Aloha, expanding its mission to bring more tools, resources, and cutting-edge robotics hardware to the research community. While the name has changed, the mission remains the same: delivering powerful, accessible, and affordable robotic solutions for AI-driven research.


Why Rebrand to Trossen AI?

The shift from Aloha to Trossen AI wasn’t just a name change—it’s a reflection of our growth, our vision for the future, and our commitment to innovation.


  1. Stronger Brand Identity – Trossen Robotics has been an industry leader in robotic manipulators, AI research hardware, and automation for over 20 years. Aligning our research line under Trossen AI strengthens our brand and unifies our growing suite of AI tools.

  2. Expanding Beyond the Original Aloha Kits – Aloha focused on core machine learning kits. Trossen AI is much more—it includes new controllers, expanded data pipelines, and an ecosystem designed for the future of robotic AI research.

  3. A Clearer Message – The name Trossen AI immediately conveys what we do: developing AI-driven robotic platforms that accelerate research, streamline data collection, and power the next generation of machine learning.

  4. Staying Ahead of the Market – The demand for low-cost, highly capable AI research hardware is growing rapidly. Trossen AI is designed to scale with that demand, ensuring that researchers and institutions have the best tools available without the high costs traditionally associated with robotics research.


More Than a Name Change—A New Era of AI Hardware

Trossen AI isn’t just replacing Aloha—it’s expanding upon it. With all-new AI hardware, software tools, and research resources, we’re setting a new standard for affordable, high-performance robotic machine learning.


Aloha Kits → Trossen AI Kits

Our new lineup of AI research kits continues the mission of Aloha while delivering more features, better performance, and a stronger ecosystem:

  • Mobile AI (Formerly Aloha Mobile)

  • Stationary AI (Formerly Aloha Stationary)

  • Solo AI (Formerly Aloha Solo)

  • WidowX AI (Leader and Follower configurations, replacing Aloha Leader-Follower Arms)


Each of these kits is built on the next-generation WidowX AI robotic manipulator, designed from the ground up for AI research and machine learning applications.


The Same Mission—Now More Powerful Than Ever

Since day one, our mission has been simple: enable groundbreaking research by making robotic AI hardware affordable and accessible. That mission continues under Trossen AI, now with even more tools, resources, and hardware advancements to support researchers, engineers, and students.


With Trossen AI, we are:

Lowering the Cost Barrier – Making high-performance robotic AI tools affordable at scale.

Bringing AI Research Out of the Lab – Enabling real-world machine learning applications with hardware designed for the next generation of automation.

Empowering Researchers and Developers – With seamless integrations, robust controllers, and advanced data pipelines, researchers can focus on AI development instead of troubleshooting hardware.

Scaling for the Future – AI and robotics research is moving beyond single-unit experimentation—we are delivering solutions for mass data collection and large-scale model training.


What’s New with Trossen AI?

While the mission remains, the technology is evolving. Trossen AI introduces a new generation of research-ready hardware with advanced controllers, servos, and AI-driven capabilities.


The WidowX AI Robotic Manipulator

At the heart of every Trossen AI kit is the WidowX AI, an all-metal, high-torque robotic manipulator designed specifically for AI research and machine learning.

Key features include:

  • Next-Generation QDD Servos – Optimized for high torque and precision while remaining lightweight.

  • Billet CNC Aluminum Construction – Engineered for durability and repeatability, built to withstand 10,000s of use cycles.

  • Integrated Cable Management – Clean, professional design with reinforced braided cables.

  • Rack & Pinion Gearset – A compact and efficient linear drive mechanism for superior grip control.


Advanced Controllers & Software for AI Development

AI research isn’t just about hardware—it’s about the entire development pipeline. Trossen AI makes data collection, model training, and model evaluation seamless with an ecosystem built for researchers, by researchers.


  • iNerve Controller – Offloads processing from the computer, delivering ultra-fast response times and real-time data processing.

  • Interbotix Driver – Built in C++ with Python bindings, making it easy to integrate with ROS, MuJoCo, NVIDIA Isaac, and Hugging Face LeRobot.

  • CAN FD High-Speed Communication – Next-gen real-time data streaming at 500Hz command rates.

  • Industrial-Grade Gravity Compensation – Hardware-based gravity modeling for enhanced precision.


Seamless Data Pipelines for AI Training

Trossen AI provides everything you need for robotic machine learning research—including native support for AI model training and evaluation.


  • Data Collection Made Simple – An intuitive touchscreen GUI makes collecting AI training data easier than ever.

  • Train on Device or in the Cloud – Train models locally using NVIDIA GPUs or offload to Google Colab for scalable cloud training.

  • Support for Common Data Formats – Easily manage datasets with Parquet and Arrow compatibility.

  • Hyperparameter Tuning – Fine-tune AI models with a simple YAML configuration, adjusting feedforward dimensions, layers, and more.


What This Means for Our Customers

If you’ve used Aloha kits, you’ll feel right at home with Trossen AI—but with even more tools, better performance, and a stronger development ecosystem.

Here’s what you can expect:

Same affordability but even more value

Upgraded hardware with cutting-edge features

Seamless software and data integrations

Ongoing support, documentation, and research resources


Looking Ahead: The Future of Trossen AI

This is just the beginning. Trossen AI represents a new era of low-cost, high-performance robotics for machine learning research. As demand for large-scale AI training environments grows, we are committed to delivering the best hardware, software, and data tools for researchers worldwide.


We look forward to seeing what the next generation of AI-powered robotics will accomplish—and we’re here to provide the tools to make it happen.


Ready to Explore Trossen AI?

👉 Visit our AI research hub now: www.trossenrobotics.com/ai

bottom of page